-dev


This option specifies the target device file with the path.

[Specification format]

-dev=[path\]file

 

-

Interpretation when omitted

When the -cpu option is specified, the specification of the CPU core type by the -cpu option becomes valid.

When the -cpu option is not specified, an error will occur.

[Detailed description]

-

This option specifies target device file file with path path.

-

The information read from the specified device file is used and an object file that matches the settings in the device file is generated.

-

An error will occur if the specified device file is not found.

-

When both this option and the -cpu option are specified and if the CPU core type in the device file specified by this option differs from that specified in the -cpu option, an error will occur.

[Example of use]

-

To specify device file "DR5F100PJ.DVF", describe as:

>asrl -dev=dr5f100pj.dvf main.asm