This option defines a user-defined assembler symbol (name).
[Specification format]
-define=name[=def][,name[=def]]...
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option specifies name as a user-defined assembler symbol (name). |
- | This is equivalent to adding "name .SET def" at the beginning of the assembly source program. |
- | An error will occur if name is omitted. |
- | If "=def" is omitted, def is regarded as 1. |
- | This option can be specified more than once. |
- | If both this option and -undefine option are specified, the option specified last will be valid. |
[Example of use]
- | To define "sample=256" as an assembler symbol, describe as: |
>asrl -define=sample=256 -dev=dr5f100pj.dvf main.asm
|