-undefine


This option deletes the assembler symbol definition by the -define option.

[Specification format]

-undefine=name[,name]...

 

-

Interpretation when omitted

None

[Detailed description]

-

This option cancels the definition of user-defined assembler symbol name specified by the -define option.

-

An error will occur if name is omitted.

-

This option cannot delete the definition by describing "name .EQU def".

-

This option can be specified more than once.

-

If both this option and -define option are specified, the option specified last will be valid.

[Example of use]

-

To delete the definition of assembler symbol "test" by the -define option, describe as:

>asrl -define=test -dev=dr5f100pj.dvf main.asm -undefine=test