-V


This option displays the version information of asrl.

[Specification format]

-V

 

-

Interpretation when omitted

Assembling is performed without displaying the version information of asrl.

[Detailed description]

This option outputs the version information of asrl to the standard error output.
It does not execute assembling.

[Example of use]

-

To output the version information of asrl to the standard error output, describe as:

>asrl -V