-help


This option displays the descriptions of asrl options.

[Specification format]

-help

 

-

Interpretation when omitted

The descriptions of asrl options are not displayed.

[Detailed description]

-

This option outputs the descriptions of asrl options to the standard error output.
It does not execute assembling.

[Example of use]

-

To output the descriptions of asrl options to the standard error output, describe as:

>asrl -help