-output


This option specifies the output file name.

[Specification format]

-output=file

 

-

Interpretation when omitted

The file is output to the current folder.

The output object file name will be the source file name with the extension replaced by ".obj".

[Detailed description]

-

This option specifies the object file name as file.

-

If file already exists, it will be overwritten.

-

Even when this option is specified, if an error occurs and assembly processing cannot be continued, no object file will be output.

-

An error will occur if two or more files are output.

-

An error will occur if file is omitted.

[Example of use]

-

To output the object file with "sample.obj" as the file name, describe as:

>asrl -output=sample.obj -dev=dr5f100pj.dvf main.asm