-g


This option outputs information for source debugging.

[Specification format]

-g

 

-

Interpretation when omitted

Information for source debugging will not be output.

[Detailed description]

-

This option outputs information for source debugging to the output file.

-

Source debugging can be performed by specifying this option.

-

When both this option and the optimization option are specified, the information output for source debugging is also affected.

[Example of use]

-

To output information for source debugging to the output file, describe as:

>ccrl -g -cpu=S2 -dev=dr5f100pj.dvf main.c