This option generates the information for inter-module optimization.
[Specification format]
- | Interpretation when omitted |
The information for inter-module optimization is not generated.
[Detailed description]
- | This option generates the additional information for inter-module optimization in the output file. |
- | At linkage, inter-module optimization is applied to files for which this option has been specified. |
[Example of use]
- | To generate the information for inter-module optimization, describe as: |
>ccrl -c -goptimize -cpu=S2 -dev=dr5f100pj.dvf main.c
|