-help


This option displays the descriptions of ccrl options.

[Specification format]

-help

 

-

Interpretation when omitted

The descriptions of ccrl options are not displayed.

[Detailed description]

-

This option outputs the descriptions of ccrl options to the standard error output.
It does not execute compilation.

[Example of use]

-

To output the descriptions of ccrl options to the standard error output, describe as:

>ccrl -help