-ignore_files_misra [Professional Edition only]


This option specifies files that will not be checked against the MISRA-C: 2004 rules or MISRA-C: 2012 rules.

[Specification format]

-ignore_files_misra=file[,file]...

 

-

Interpretation when omitted

All C source files are checked.

[Detailed description]

-

This option does not check file file against the MISRA-C: 2004 rules or MISRA-C: 2012 rules.

-

This option is valid only when the -misra2004 or -misra2012 option is specified.
If the -misra2004 or -misra2012 option is not specified, a warning is output and this option will be ignored.

[Example of use]

-

Not to check sample.h against the MISRA-C: 2004 rules, describe as:

>ccrl -misra2004=all -ignore_files_misra=sample.h -cpu=S2 -dev=dr5f100pj.dvf main.c

[Caution]

-

An error will occur when this option is specified in the Standard Edition of the compiler.