-dev


This option specifies the device file that the assembler and optimizing linker use.

[Specification format]

-dev=file

 

-

Interpretation when omitted

No device file is passed to the assembler or optimizing linker.

[Detailed description]

-

This option specifies device file file that the assembler and optimizing linker use.

-

If this option is omitted at compilation, an error may occur in the assembler or the optimizing linker.

-

An error will occur if this option is specified more than once.

-

An error will occur if file is omitted.

[Example of use]

-

To specify device file "DR5F100PJ.DVF" that the assembler and optimizing linker use, describe as:

>ccrl -cpu=S2 -dev=dr5f100pj.dvf main.c