This option specifies options with a subcommand file.
Option contents specified with a subcommand file are expanded to the location at which this option is specified on the command line and are executed. |
See "2.4.2 Subcommand file usage" for details about a subcommand file. |
input file2.obj file3.obj ; This is a comment. library lib1.lib, & ; This is a line continued. lib2.lib |
To specify subcommand file sub.txt, describe as:
The command line is expanded as follows, and the file input order is: file1.obj, file2.obj, file3.obj, file4.obj.