-END


This option executes option strings specified before this option.

[Specification format]

-END

 

-

Interpretation when omitted

None

[Detailed description]

-

This option executes option strings specified before this option.
After link processing is terminated, option strings specified before this option are input and link processing is continued.

[Caution]

-

This option can be used only in a subcommand file.

[Example of use]

-

Create subcommand file "sub.txt" with the following content.

input=a.obj,b.obj                       ;(1)
start=.SEC1,.SEC2,.SEC3/100,.SEC4/8000  ;(2)
output=a.abs                            ;(3)
end
input=a.abs                             ;(4)
form=stype                              ;(5)
output=a.mot                            ;(6)

 

To specify subcommand file sub.txt, describe as:

>rlink -subcommand=sub.txt

 

Processing from (1) to (3) are executed and a.abs is output.

Then processing from (4) to (6) are executed and a.mot is output.