3.2.10 Vector table address information

When the -show=vector option is specified, the contents of the vector table addresses is output.

The output example of the vector table address information is shown below.

*** Variable Vector Table List ***
(1)     (2)
ADDRESS SYMBOL/ADDRESS
00      start
02      dummy
04      INTWDTI
06      0000F100
 :

Number

Description

(1)

Vector table address

The vector table address is output.

(2)

Symbol

The symbol is output.

When no symbol is specified, the address is output.