Renesas Electronics
The version information of the optimizing linker and the time of linkage are output.
The output example of the header information is shown below.
Renesas Optimizing Linker (VX.XX.XX) XX-Xxx-XXXX XX:XX:XX (1)
Number
Description
(1)
Version information of the optimizing linker and time of linkage