Renesas Electronics
The following byte separation operators are available.
Operator
Overview
HIGH
Obtains the second byte from the least significant byte of a term
LOW
Returns the low-order 8-bit value of a term