LOW


Returns the low-order 8-bit value of a term.

[Function]

Returns the value of the lower-order eight bits among the 32 bits of a term.

[Application example]

MOV     A, #LOW(0x1234)         ; (1)

(1)

By executing a MOV instruction, this operator loads the low-order 8-bit value "0x34" of the expression "0x1234" to A register.