+


Addition of values of first and second terms.

[Function]

Returns the sum of the values of the 1st and 2nd terms of an expression.

[Application example]

START:  BR      !!START + 6     ; (1)

(1)

The BR instruction causes a jump to "address assigned to START plus 6", namely, to address "0x100 + 0x6 = 0x106" when START label is 0x100.