-


Subtraction of value of first and second terms.

[Function]

Returns the result of subtraction of the 2nd-term value from the 1st-term value.

[Application example]

BACK:   BR      !!BACK - 6      ; (1)

(1)

The BR instruction causes a jump to "address assigned to BACK minus 6", namely, to address "0x100 - 0x6 = 0xFA" when BACK label is 0x100.