This section describes behavior that is not specified by the ANSI standard.
Static data is output during compilation as a data section.
This is dependent on the design of the display device.
Conforms to IEC 60559:1989 (IEEE754Note-1985).
IEEE: Institute of Electrical and Electronics Engineers |
Note that the default size for the double and long double types is 32 bits. When the -dbl_size=8 option is used, the default size is 64 bits.
See "(8)Bit field" for the boundary alignment of structure objects with bit fields.
Formal parameters are allocated to registers. For the details of description, see "9.1Function Call Interface".