11.1.4 Data flash area

The CC-RL does not output code to the data flash area.

Use assembler code for access to the data flash area.

In case of writing codes in C language, use 8-bit data to access the area.