To output bit manipulation instructions without using embedded functions, satisfy all conditions shown below.
The value is assigned to a single-bit bit field of the charunsigned charsigned char_Bool type in the near area. |
For a variable qualified with volatile, the compiler does not output a bit manipulation instruction when a value is assigned to the variable or when the variable is read unless the other conditions are satisfied. For a variable that is not qualified with volatile, the compiler outputs a bit manipulation instruction according to the specified optimization settings.