Interrupt handler for RTOS (#pragma rtos_interrupt)
|
The interrupt handler for Renesas RTOS for the RL78 family can be specified.
[Function]
- | Interprets the function name specified with the #pragma rtos_interrupt directive as the interrupt handler for Renesas RTOS for the RL78 family. |
- | When the vector table is specified, the address of the described function name is registered in the specified interrupt vector table. |
- | The code for the body (function definition) of an interrupt handler is output to the .text or .textf section.
The section name can be changed through #pragma section.
Note however when the vector table is specified, the start address of the interrupt handler should be a location that can be accessed in 16-bit addressing. |
- | When the vector table is specified, the specification becomes __near forcibly, regardless of whether __far is specified explicitly or implicitly. No warning message is output. |
- | When the vector table is not specified, the __near or __far specification by the function takes priority, regardless of whether the specification is explicit or implicit. |
- | The interrupt handler for RTOS generates codes in the following order. |
(a) | Calls kernel symbol __kernel_int_entry using call !!addr20 instruction
When the vector table is specified, the interrupt address is passed to __kernel_int_entry as an argument.
When the vector table is not specified, no argument is passed to __kernel_int_entry. |
(b) | Secures the local variable area (only when there is a local variable) |
(c) | Executes the body of the function |
(d) | Releases the local variable area (only when there is a local variable) |
(e) | Unconditionally jumps to label _ret_int using br !!addr20 instruction |
[Effect]
- | The interrupt handler for RTOS can be described in the C source level. |
[Usage]
- | The interrupt address and function name is specified by the #pragma directive. |
#pragma rtos_interrupt [(]function-name[(vect=addressNote)][)]
|
Note | address : Binary, octal, decimal, or hexadecimal constant
Only an even value from 0 to 0x7c can be specified as the constant
(a value outside this range will cause an error). |
- | Write a #pragma directive before the function definition. |
[Restrictions]
- | If the function specified with #pragma rtos_interrupt is called in the same way as a normal function, a compilation error will occur. |
#pragma rtos_interrupt func (vect=8)
void func(void) {}
void xxx()
{
func(); //Error
}
|
- | The parameters and return value of a function should be declared as void (e.g., void func (void);).
If the type is not void, a compilation error will occur. |
- | If an interrupt handler for RTOS is specified with __inline, __callt or another type of #pragma, a compilation error will occur. |
- | After the #pragma rtos_interrupt declaration line, a call or a definition of _kernel_int_exit or _kernel_int_entry as a function or a variable will generate an error. |
#pragma rtos_interrupt func (vect=8)
void func(void) {
_kernel_int_entry(); //Error
_kernel_int_exit(); //Error
}
void _kernel_int_entry(){} //Error
void _kernel_int_exit(){} //Error
|
[Example]
The following shows an example in which the vector table is specified and no function is called in an interrupt handler.
[ Input program ]
#include "iodefine.h"
#pragma rtos_interrupt inthdr (vect=INTP0)
volatile int g;
void inthdr(void) {
volatile int a;
a = 1;
g = 1;
}
|
[ Output program ]
.SECTION .textf,TEXTF
_inthdr .vector 0x0008
_inthdr:
push ax ;ax register is saved
movw ax, #0x0008
call !!__kernel_int_entry ;Registers other than ax are saved
push hl ;The area for local variables is allocated
onew ax
movw [sp+0x00], ax
movw !LOWW(_g), ax
pop hl ;The area for local variables is released
br !!__kernel_int_exit ;Processing is specified so that all registers
;are restored when the interrupted task
;resumes execution
|
The following shows an example in which the vector table is not specified and no function is called in an interrupt handler.
[ Input program ]
#include "iodefine.h"
#pragma rtos_interrupt inthdr
volatile int g;
void inthdr(void) {
volatile int a;
a = 1;
g = 1;
}
|
[ Output program ]
.SECTION .textf,TEXTF
_inthdr:
call !!__kernel_int_entry ;Registers other than ax are saved
push hl ;The area for local variables is allocated
onew ax
movw [sp+0x00], ax
movw !LOWW(_g), ax
pop hl ;The area for local variables is released
br !!__kernel_int_exit ;Processing is specified so that all registers
;are restored when the interrupted task
;resumes execution
|