memchr


Character search from object

[Classification]

Standard library

[Syntax]

#include <string.h>

void __near * __far memchr(const void __near *s, int c, size_t n);

void __far * __far _COM_memchr_f(const void __far *s, int c, size_t n);

[Return value]

If c is found, a pointer indicating this character is returned. If c is not found, the null pointer is returned.

[Description]

This function obtains the position at which character c appears first in the first n number of characters in an object indicated by s.