8.2.7 Startup of main function

The main function is called when all processings that need to be performed by the startup routine have finished.

Write the following instruction to call the main function.

CALL    !!_main