8.2.2 Register bank setting

Since the register bank is initialized to RB0 at a reset, set the register bank as follows only when desiring to set the work register to a register bank other than RB0.

This processing cannot be written for the RL78-S1 core because it does not have the SEL instruction.

SEL     RB1