10.2 Message Formats

This section describes the output formats of messages.

The output formats of messages are as follows.

(1)

When the file name and line number are included

file-name (line-number) : message-type 05 message-number : message

(2)

When the file name and line number aren't included

message-type 05 message-number : message

Remark

Following contents are output as the continued character string.

Message Types : 1 alphabetic character
Message Numbers : 5 digits