10.3 Message Types

This section describes the message types displayed by CC-RL.

The message types (1 alphabetic character) are as follows.

Table 10.1

Message Type

Message Type

Description

C

Internal error : Processing is aborted.

No object codes are generated.

E

Error : Processing is aborted if a set number of errors occur.

No object codes are generated.

F

Fatal error : Processing is aborted.

No object codes are generated.

M

Information : Processing continues.

Object codes are generated.

W

Warning : Processing continues.

Object codes are generated (They might not be what the user intended).