This section describes the options for the RX family C/C++ compiler in each processing phase.
Compile phase: Refer to 2.5.1 Compile Options.
Assembly phase: Refer to 2.5.2 Assembler Command Options.
Link phase: Refer to 2.5.3 Optimizing Linkage Editor (rlink) Options.
Library generation phase: Refer to 2.5.4 Library Generator Options.