2.5.4 Library Generator Options

Classification

Option

Description

Library Options

-head

Specifies a configuration library.

-output

Specifies an output library file name.

-nofloat

Creates a simple I/O function.

-reent

[To be supported by V2.03 and later versions]

Creates a reentrant library.

-lang

Selects the set of functions available from the C standard library.

-simple_stdio

Creates a functionally cut down version of the set of I/O functions.

-secure_malloc [Professional Edition only] [V2.05.00 or later]

Generates the calloc, free, malloc and realloc with security facility.

-logo
-nologo

Outputs the copyright.

Disables output of the copyright.