< Compile Options / Object Options >
A local label and nop instruction are not inserted.
This option inserts a local label and nop instruction at the specified location based on the information for source debugging. |
This function is assumed to be used via CS+ or e2studio and should not be used directly by the user. |