-asmcmd


< Compile Options / Assemble and Linkage Options >

[Format]

-asmcmd=<file name>

[Description]

-

This option specifies the assembler options to pass to asrx with a subcommand file.

[Example]

ccrx -isa=rxv1 -asmcmd=file.sub sample.c

The above description has the same meaning as the following two command lines:

ccrx -isa=rxv1 -output=src sample.c
asrx -isa=rxv1 -subcommand=file.sub sample.src

[Remarks]

-

If this option is specified for more than one time, all specified subcommand files are valid.