Renesas Electronics
-chkfpu
< Assembler Command Options / Source Options >
[Format]
[Description]
-
This option outputs warning W0551012 when a floating-point operation instruction is used in the source file.
[Remarks]
For details of the floating-point operation instructions, refer to the RX Family Software Manual.