< Assembler Command Options / Other Options >
When the subcommand option is specified, the assembler options specified in a subcommand file are used at assembler startup. Specify options in a subcommand file in the same format as in the command line. |
When options are specified in the command line as shown (1) below, the assembler interprets them as shown in (2). |