< Optimizing Linkage Editor (rlink) Options / Optimize Options >
When this option is omitted, the default is samesize=1E.
Specifies the minimum code size for the optimization with the same-code unification (optimize=same_code). Specify a hexadecimal value from 8 to 7FFF. |