< Optimizing Linkage Editor (rlink) Options / Subcommand File Option >
[Format]
-subcommand = <file name>
|
[Description]
- | Specifies options with a subcommand file. |
- | The format of the subcommand file is as follows:
<option> { = | Δ } [<suboption> [,…] ] [ Δ&] [;<comment>] |
- | The option and suboption are separated by an "=" sign or a space. |
- | For the input option, suboptions are separated by a space. |
- | One option is specified per line in the subcommand file. |
- | If a subcommand description exceeds one line, the description can be allowed to overflow to the next line by using an ampersand (&). |
[Examples]
- | Command line specification: |
rlink file1.obj -sub=test.sub file4.obj
|
- | Subcommand specification: |
input file2.obj file3.obj ; This is a comment.
library lib1.lib, & ; Specifies line continued.
lib2.lib
|
- | Option contents specified with a subcommand file are expanded to the location at which the subcommand is specified on the command line and are executed. |
- | The order of file input is file1.obj, file2.obj, file3.obj, and file4.obj. |