Table 3-3 shows the structure and contents of the linkage list.
When -show OptionNote is Specified |
When -show Option is not Specified |
|||
When -show=relocation_attribute is specified, the relocation attribute is output. |
-show=relocation_attribute |
|||
Static definition symbol name, address, size, and type in the order of address When -show=reference is specified: Symbol reference count and optimization information in addition to the above information When -show=struct is specified, information on the structure and union members is output. |
-show =symbol -show =reference |
|||
-show =symbol |
||||
-show =xreference |
||||
-show=total_size |
||||
-show=vector |
||||
Contents of the function list for use in detecting illegal indirect function calls |
-show=cfi |
The -show option is valid when the list option is specified. |