3.2.6 Symbol Deletion Optimization Information

The size and type of symbols deleted by symbol deletion optimization (-optimize=symbol_delete) are output.

The following figure shows an example of symbol deletion optimization information output.

*** Delete Symbols ***
(1)                            (2)    (3)
SYMBOL                         SIZE   INFO
  _Version
                                  4   data ,g

Item Number

Description

(1)

Deleted symbol name

(2)

Deleted symbol size

(3)

Deleted symbol type as shown below

Data type

func: Function name

data: Variable name

Declaration type

g: External definition

l: Internal definition