Renesas Electronics
The option strings specified by a command line or a subcommand file are output.
The following figure shows an example of option information output when rlink -subcommand = test.sub -list -show is specified.
Item Number
Description
(1)
Outputs option strings specified by a command line or a subcommand in the specified order.
(2)
Subcommand in the test.sub subcommand file.