The RXC supports the language specifications stipulated by the ANSI standards. These specifications include items that are stipulated as processing definitions. This chapter explains the language specifications of the items dependent on the processing system of the RX microcontrollers.
For extended language specifications explicitly added by the RXC, refer to section 4.2 Extended Language Specifications.