4.1.6
Conforming Language Specifications
(1) | C Language Specifications (When the lang=c Option is Selected) |
ANSI/ISO 9899-1990 American National Standard for Programming Languages -C
(2) | C Language Specifications (When the lang=c99 Option is Selected) |
ISO/IEC 9899:1999 INTERNATIONAL STANDARD Programming Languages - C
(3) | C++ Language Specifications (When the lang=cpp Option is Selected) |
Based on the language specifications compatible with Microsoft® Visual C/C++ 6.0