The following shows the mnemonic line format.
[label][operation[Δoperand(s)]][comment]
Define a name for the address of the mnemonic line.
Write a mnemonic or a directive.
Write the object(s) of the operation. The number of operands and their types depend on the operation. Some operations do not require any operands.
Write notes or explanations that make the program easier to understand.