Go to the Location dialog box


This dialog box is used to move the caret to a specified position.

Figure A.52

Go to the Location Dialog Box

 

This section describes the following.

[How to open]

-

Focus the Disassemble panel, and then select [Go to…] from the [Edit] menu.

-

Focus the IOR panel, and then select [Go to…] from the [Edit] menu.

-

On the Disassemble panel, select [Go to…] from the context menu.

-

On the IOR panel, select [Go to…] from the context menu.

[Description of each area]

(1)

[Address/Symbol], or [IOR] area

Specify the location to which the caret jumps.

You can either type a location directly into the text box (up to 1024 characters), or select one from the input history via the drop-down list (up to 10 items).

The data to specify various depending on the target panel, as follows:

Target Panel

Data Specified

Disassemble panel

Address expression

IOR panel

I/O register name

Remark

If this dialog box is opened from the Disassemble panel, a symbol name at the current caret position can be complemented by pressing the [Ctrl] + [Space] key in this text box (see "2.20.2 Symbol name completion function").

[Function buttons]

Button

Function

OK

Moves the caret to the specified location, from the beginning of the area displayed in the target panel.

Cancel

Cancels the jump and closes this dialog box.

Help

Displays the help for this dialog box.