Select I/O Modules dialog box


This dialog box is used to set the I/O modules which details are displayed.

Figure A.30

Select I/O Modules Dialog Box

 

The following items are explained here.

[How to open]

-

On the [Debug Tool Settings] tab of the Property panel, click the [...] button displayed by selecting one of the values of the [I/O modules] property in the [Memory] category.

[Description of each area]

(1)

Area for specifying I/O module name

This area displays a list of the names of I/O modules defined in the device file.

(a)

[Module Name]

This area displays the names of I/O modules which are defined in the device file.

If any of the check boxes is selected, the I/O modules are used for debugging.

[Function buttons]

Button

Function

OK

Closes this dialog box and calls the settings to reflect them in the previous properties.

Initialize All Settings

Sets all check boxes under [Module Name] settings to their default values.

Cancel

Cancels the settings and closes this dialog box.

Help

Displays the help of this dialog box.