The number of events that can be set to Valid state at the same time are subject to the following limitations.
Consequently, if enabling a new event would exceed the limit, you must first set some other event to Invalid state.
| 
 
Performance Measurement   | 
|||
"x + y": "Hardware Break (execution type): x" + "Hardware Break (access type): y"
Among Hardware Break (execution type: before execution) events, four events are shared with Hardware Break (access type) events (e.g. when four Hardware Break (access type) events are used, only eight hardware break (execution type: before execution) events can be used).  |