2.18.6.2  
Event types that can be set and deleted during execution
 
The following types of events can be set or deleted during program execution, or during tracer/timer execution.
Table 2.22  | Event Types That Can be Set and Deleted during Execution   | 
 
| 
 | 
 | 
| 
 | 
 | 
 | 
| 
 
Hardware Break  
(execution type: after execution)  
 | 
 | 
 | 
| 
 
Hardware Break  
(execution type: before execution)  
 | 
 | 
 | 
| 
 
Hardware Break  
(access type)  
 | 
 | 
 | 
| 
 
Software Break 
 | 
 | 
 | 
| 
 
Trace  
(trace start/trace end) 
 | 
 | 
 | 
| 
 
Point Trace 
 | 
 | 
 | 
| 
 
Timer Result 
(timer start/timer end) 
 | 
 | 
 | 
| 
 
Performance Measurement  
(performance measurement start/ 
performance measurement end) 
 | 
 | 
 | 
| 
 
Action  
(Printf) 
 | 
 | 
 | 
 
 
 		: Possible, if the program execution is allowed to pause for eventsNote
 		: Impossible while tracer or timer is executing 
NG 		: Impossible
 		: Not supported
Note  | To enable this, specify [Yes] with the [Set event by stopping execution momentarily] property in the [Set Event While Running] category on the [Debug Tool Settings] tab of the Property panel.   |