2.1 Overview

The Code Generator is used to output report files such as a device list view and a device top view.

The following sections describe the operation procedures for Code Generator.

(1)

Start CS+

Launch CS+ from the [Start] menu of Windows.

(2)

Create/Open project

Create a new project (that defines a kind of project, microcontroller to be used, build tools to be used, etc.) or load an existing project.

Open the Device List View panel, where you enter information on the pins of the microcontroller.

Open the Device Top View panel, where you can confirm the information entered for the pins.

Allows you to select colors used to distinguish the type of pins whose information is displayed in the Device Top View panel.

Output report files (files containing configured information using Code Generator: device list view and device top view) to the specified folder.

Output a device list view.

Output a device top view.

(6)

Save project

Save a project.