Project Tree panel


This panel displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

Figure A.2

Project Tree Panel

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Project Tree].

[Description of each area]

(1)

Project tree area

This area displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

(a)

Code Generator (Design Tool) - Pin View

This node consists of the following pin nodes.

Device List View

Opens the Device List View panel.

Device Top View

Opens the Device Top View panel.

[Context menu]

Property

Opens the Property panel corresponding to the selected node.