[Device Top View Settings] tab


This panel allows you to view the information (Device top view color setting) on and change the setting for the node selected in the Project Tree panel.

Figure A.6

[Device Top View Settings] Tab

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device Top View], and then select [Property] from the [View] menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device Top View], and then select [Property] from the context menu.

Remark

If this panel is already open, selecting a different [Device Top View] in the Project Tree panel changes the content displayed accordingly.

[Description of each area]

(1)

[Device top view color setting] category

Select the display colors to differentiate the pin groups (Device, Device group text, etc.) in the device top view.

Device

Selects the display color of the microcontroller.

Device group text

Selects the display color of the device group.

Device part number text

Selects the display color of the device part number.

Macro highligh

Selects the background color of pins selected in the Device List View panel, on the [Macro] tab.

Selected pin

Selects the background color of a pin selected in the Device List View panel, on the [Pin Number] tab.

Unused pins

Selects the display color for unused pins (dual-use pins with no use set in the Device List View panel).

Used pins

Selects the display color for used pins (dual-use pins with a use set in the Device List View panel).