|
debugger.ActionEvent.GetLine
|
This property sets or refers to the number of action event results.
[Specification format]
debugger.ActionEvent.GetLine = number
|
[Setting(s)]
|
|
|
|
number
|
Set the number of action event results that can be held in the Python console (default: 10000).
|
[Reference]
Current set value
[Detailed description]
- | This property sets or refers to the number of action event results that can be held in the Python console. |
- | If the number that was set is exceeded, action event results cannot be held. Deletion is performed from old action events. The valid range is from 5000 to 100000. |
[Example of use]
>>>print debugger.ActionEvent.GetLine
10000
>>>debugger.ActionEvent.GetLine = 50000
>>>print debugger.ActionEvent.GetLine
50000
|